Choose language

TE 1000-AVR

Original operating instructions

Information about the documentation

About this documentation

  • Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
  • Observe the safety instructions and warnings in this documentation and on the product.
  • Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.

Explanation of symbols used

Warnings

Warnings alert persons to hazards that may occur when handling or using the product. The following signal words are used in combination with a symbol:
Image alternative DANGER! Draws attention to an imminent hazard that will lead to serious personal injury or fatality.
Image alternative WARNING! Draws attention to a potential hazard that could lead to serious personal injury or fatality.
Image alternative CAUTION! Draws attention to a potentially dangerous situation that could lead to minor personal injury or material damage.

Symbols in the documentation

The following symbols are used in this document:
Image alternative Read the operating instructions before use
Image alternative Instructions for use and other useful information

Symbols in the illustrations

The following symbols are used in illustrations:
Image alternative These numbers refer to the corresponding illustrations found at the beginning of these operating instructions.
Image alternative The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text.
Image alternative Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section.
Image alternative This symbol is intended to draw special attention to certain points when handling the product.

Symbols on the product

Symbols on the product

The following symbols are used on the product:
Image alternative Protection class II (double-insulated)

Product information

Hilti products are designed for professional use and may be operated, serviced and maintained only by trained, authorized personnel. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
  • Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
    Product information
    Breaker
    TE 1000‑AVR
    Generation
    02
    Serial no.

Declaration of conformity

We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany

Safety

General power tool safety warnings

Image alternative WARNING
Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference.
The term “power tool” in the warnings refers to your mains-operated (corded) power tool or battery-operated (cordless) power tool.
Work area safety
  • Keep work area clean and well lit. Cluttered or dark areas invite accidents.
  • Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
  • Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
Electrical safety
  • Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
  • Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
  • Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
  • Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
  • When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
  • If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
Personal safety
  • Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
  • Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
  • Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
  • Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
  • Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
  • Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
  • If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
Power tool use and care
  • Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
  • Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
  • Disconnect the plug from the power source and/or the battery pack from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
  • Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
  • Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
  • Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
  • Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
Service
  • Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.

Hammer safety warnings

  • Wear ear protectors. Exposure to noise can cause hearing loss.
  • Use auxiliary handles, if supplied with the tool. Loss of control can cause personal injury.
  • Hold power tool by insulated gripping surfaces, when performing an operation where the cutting accessory may contact hidden wiring or its own cord. Cutting accessory contacting a "live" wire may make exposed metal parts of the power tool "live" and could give the operator an electric shock.

Additional safety instructions

Personal safety
  • Use the product only when it is in technically faultless condition.
  • Never tamper with or modify the tool in any way.
  • Apply appropriate safety measures at the opposite side of the workpiece in work that involves breaking through. Parts breaking away could fall out and / or fall down causing injury to other persons.
  • Check that the side handle is fitted correctly and tightened securely. Always hold the tool securely with both hands on the grips provided. Keep the grips dry, clean and free from oil and grease.
  • Take breaks between working and do physical exercises to improve the blood circulation in your fingers. Exposure to vibration during long periods of work can lead to disorders of the blood vessels and nervous system in the fingers, hands and wrists.
  • The tool is not intended for use by debilitated persons who have received no special training.
  • Keep the power tool out of reach of children.
  • Before beginning the work, check the hazard classification of the dust that will be produced. Use an industrial vacuum cleaner with an officially approved protection classification in compliance with locally applicable dust protection regulations.
  • Use a dust removal system and suitable vacuum cleaner whenever possible. Dust from materials, such as paint containing lead, some wood species, concrete/masonry/stone containing silica, and minerals as well as metal, may be harmful.
  • Make sure that the workplace is well ventilated and, where necessary, wear a respirator appropriate for the type of dust generated. Contact with or inhalation of the dust may cause allergic reactions and/or respiratory or other diseases to the operator or bystanders. Certain kinds of dust are classified as carcinogenic such as oak and beech dust, especially in conjunction with additives for wood conditioning (chromate, wood preservative). Material containing asbestos may be handled only by specialists.
  • Approval must be obtained from the site engineer or architect prior to beginning the work. Work on buildings and other structures may influence the statics of the structure, especially when steel reinforcing bars or load-bearing components are cut through.
Electrical safety
  • Before beginning work, check the working area for concealed electric cables or gas and water pipes. External metal parts of the power tool may give you an electric shock if you damage an electric cable accidentally.
  • Check the power tool’s supply cord at regular intervals and have it replaced by a qualified specialist if found to be damaged. If the power tool’s supply cord is damaged it must be replaced with a specially-prepared and approved supply cord available from Hilti Customer Service. Check extension cords at regular intervals and replace them if found to be damaged. Do not touch the supply cord or extension cord if it is damaged while working. Disconnect the supply cord plug from the power outlet. Damaged supply cords or extension cords present a risk of electric shock.
  • Dirty or dusty power tools that have been used frequently for work on conductive materials should be checked at regular intervals at a Hilti Service Center. Dust (especially dust from conductive materials) or dampness adhering to the surface of the power tool may, under unfavorable conditions, lead to electric shock.
  • Switch the power tool off and unplug the supply cord in the event of a power failure or interruption in the electric supply. This will prevent accidental restarting when the electric power returns.

Description

Product overview

Image alternative
  1. Chuck
  2. Air vents
  3. Side handle
  4. Knob
  5. On/off switch
  6. Grip
  7. Power level selector switch
  8. Connector on electric tool
  9. Supply cord with keyed, releasable plug connector
  10. Service indicator
  11. Power level indicator

Intended use

The product described is an electrically powered breaker for heavy chiseling work.

It is designed for breaking or demolishing concrete, masonry, stone and asphalt.
  • Operation is permissible only when connected to a power source providing a voltage and frequency in compliance with the information given on the type identification plate.

Possible misuse

This product is not suitable for working on hazardous materials.
This product is not suitable for working in a damp environment.

Active Vibration Reduction (AVR)

The breaker is equipped with an Active Vibration Reduction (AVR) system, which reduces vibration significantly.

Power level indicator

The breaker is equipped with a power level indicator LED.
Chiseling power can be reduced to approx. 70% by pressing the power level selector switch. The power level LED then lights up, indicating reduced power.

Service indicator information

The breaker is equipped with a service indicator LED.
Status
Meaning
The service indicator lights red.
End of service interval – servicing is due.
A fault has occurred in the tool.
The service indicator blinks red.
The overheating prevention cut-out has been activated.
The voltage provided by the electric supply is too high.
Bring the product to Hilti Service in good time. This will help to ensure that it’s always ready for use.

Items supplied

Breaker, side handle, operating instructions.
You can find other system products approved for your product at your local Hilti Center or online at: www.hilti.group .

Technical data

Breaker

For details of the rated voltage, current, frequency and/or input power, please refer to the power tool’s country-specific type identification plate.
When powered by a generator or transformer, the generator or transformer’s power output must be at least twice the rated input power shown on the rating plate of the power tool. The operating voltage of the transformer or generator must always be within +5% and -15% of the rated voltage of the power tool.

TE 1000‑AVR
Weight in accordance with EPTA procedure 01
12.5 kg
Single impact energy in accordance with EPTA procedure 05
26 J

Noise information and vibration values in accordance with EN 62841

The sound pressure and vibration values given in these instructions were measured in accordance with a standardized test and can be used to compare one power tool with another. They can also be used for a preliminary assessment of exposure.
The data given represent the main applications of the power tool. However, if the power tool is used for different applications, with different accessory tools, or is poorly maintained, the data can vary. This can significantly increase exposure over the total working period.
An accurate estimation of exposure should also take into account the times when the tool is switched off, or when it is running but not actually being used for a job. This can significantly reduce exposure over the total working period.
Identify additional safety measures to protect the operator from the effects of noise and/or vibration, for example: maintaining the power tool and accessory tools, keeping the hands warm, organization of work patterns.
Noise emission values
Sound (power) level (LWA)
96 dB(A)
Uncertainty for the sound power level (KWA)
3 dB(A)
Emission sound pressure level (LpA)
85 dB(A)
Uncertainty for the sound pressure level (KpA)
3 dB(A)
Noise information and vibration values
Chiseling (ah, Cheq)
5 m/s²
Uncertainty (K)
1.5 m/s²

Operation

Preparations at the workplace

CAUTION
Risk of injury! Inadvertent starting of the product.
  • Unplug the supply cord before making adjustments to the power tool or before changing accessories.
Observe the safety instructions and warnings in this documentation and on the product.

Fitting and adjusting the side handle

CAUTION
Risk of injury! Loss of control over the breaker.
  • Check that the side handle is fitted correctly and tightened securely.
Image alternative
  • Fit or adjust the side handle.
    The instructions provided with the side handle must also be observed.

Detachable supply cord

CAUTION
Risk of injury! Due to leakage current as a result of dirty contacts.
  • Connect the detachable electric connector to the electric tool only when it is clean and dry and when the supply cord is unplugged from the power outlet.
  • Connect / disconnect the detachable supply cord.

Connecting the detachable supply cord

CAUTION
Risk of injury! Due to leakage current as a result of dirty contacts.
  • Connect the detachable electric connector to the electric tool only when it is clean and dry and when the supply cord is unplugged from the power outlet.
  1. Push the keyed, detachable electric plug connector into the socket as far as it will go, until it is heard to engage.
  2. Plug the supply cord into the power outlet.

Disconnecting the detachable supply cord

  1. Unplug the supply cord from the power outlet.
  2. Press the release button and pull the keyed, detachable electric plug connector out of the socket.
  3. Pull the supply cord connector out of the power tool.

Fitting the accessory tool

Image alternative
  1. Apply a little grease to the connection end of the accessory tool.
  2. Push the accessory tool into the chuck as far as it will go, turning it and applying light pressure until it engages with an audible click.
    • The product is ready for use.
    Use only the recommended grease supplied by Hilti . Use of unsuitable grease may cause damage to the product.

Removing the accessory tool

WARNING
Risk of injury! The accessory tool gets hot during use and may also have sharp edges.
  • Wear protective gloves when changing the tool.
DANGER
Risk of fire! Risk of contact between the hot accessory tool and highly inflammable materials.
  • Do not lay the hot accessory tool down on highly inflammable materials.
Image alternative
  1. Pull the chuck back.
  2. Remove the accessory tool.

Types of work

ATTENTION
Risk of damage by incorrect handling!
  • Do not operate the switches for direction of rotation and/or function selection during operation.
Observe the safety instructions and warnings in this documentation and on the product.

Chiseling

The chisel can be adjusted to 6 different positions (in 60° increments). This ensures that flat chisels and shaped chisels can always be set to the optimum working position.
If inadequate pressure is applied, the chisel will jump around uncontrollably. Application of excessive pressure will result in a loss of chiseling performance.
Image alternative
  1. Plug the supply cord into the power outlet.
  2. Bring the chisel into contact with the workpiece about 80 -100 mm (3¹⁄₈" - 4") from its edge.
  3. Begin with the chisel positioned at an angle of 70° to 80° to the concrete surface, with the tip of the chisel pointing toward the edge of the workpiece. Break material away by subsequently increasing the angle to approx. 90° as the chisel penetrates.
    • When working close to reinforcing bars, always guide the tip of the chisel toward the edge of the workpiece, not toward a reinforcing bar.
  4. Rotate the chisel regularly to help ensure even wear and to promote the self-sharpening process.

Setting the chiseling power

  • Press the power level selector switch.
    • Chiseling power can be reduced to approx. 70% by pressing the power level selector switch.
    Chiseling power can be adjusted only when the power tool is switched on and ready for use. To reselect full chiseling power, press the chiseling power level selector switch again. Switching off and then on again also causes the power tool to return to full chiseling power.

Care and maintenance

WARNING
Electric shock hazard! Attempting care and maintenance with the supply cord connected to a power outlet can lead to severe injury and burns.
  • Always unplug the supply cord before carrying out care and maintenance tasks.
Care
  • Carefully remove any dirt that may be adhering to parts.
  • Clean the air vents carefully with a dry brush.
  • Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these may attack the plastic parts.
Maintenance
WARNING
Danger of electric shock! Improper repairs to electrical components may lead to serious injuries including burns.
  • Repairs to the electrical section of the tool or appliance may be carried out only by trained electrical specialists.
  • Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
  • Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
  • After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by Hilti for use with the product can be found at your local Hilti Store or online at: www.hilti.group .

Cleaning the dust shield

  • Clean the dust shield on the chuck with a dry, clean cloth at regular intervals.
  • Clean the sealing lip by wiping it carefully and then grease it again lightly with Hilti grease.
  • It is essential that the dust shield is replaced if the sealing lip is damaged.

Transport and storage

  • Do not transport electric tools with accessory tools fitted.
  • Always unplug the supply cord before storing an electric tool or appliance.
  • Store tools and appliances in a dry place where they cannot be accessed by children or unauthorized persons.
  • Check electric tools or appliances for damage after long periods of transport or storage.

Troubleshooting

If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.

Troubleshooting

Trouble or fault
Possible cause
Action to be taken
The power tool doesn’t start.
Electronics initialization in progress (takes up to 4 seconds after plugging in). The electronic restart interlock is activated after an interruption in the electric supply.
  • Switch the power tool off and then on again.
Interruption in the electric supply.
  • Plug in another electric tool or appliance and check whether it works.
The generator is in sleep mode.
  • Apply a load to the generator by connecting a second power consumer (e.g. worklight). Switch the tool off and then on again.
The detachable supply cord is not fitted correctly.
  • Fit the detachable supply cord to the power tool correctly.
The service indicator lights red.
The tool is faulty or servicing is due.
  • Have the product repaired only by Hilti Service.
The service indicator blinks red.
The voltage provided by the electric supply is too high.
  • Use a different power outlet. Check the electric supply.
The overheating prevention cut-out has been activated.
  • Allow the tool to cool down. Clean the air vents. Running under no load is still possible.
No hammering action.
The power tool is too cold.
  • Bring the tip of the accessory tool into contact with the working surface, switch the power tool on and allow it to run. If necessary, repeat the procedure until the hammering mechanism begins to operate.
The tool does not achieve full power.
Power reduction is active.
  • Press the power level selector switch (observe the power level indicator). Unplug the power tool from the electric supply and then plug it back in.
The extension cord is too long or its gauge is inadequate.
  • Use an extension cord of an approved length and / or of adequate gauge.
The voltage provided by the electric supply is too low.
  • Connect the power tool to a different power source.
The chisel cannot be released from the chuck.
The chuck is not pulled back fully.
  • Pull the chuck back as far as it will go and remove the insert tool.
The power tool switches itself off while running.
The overheating prevention cut-out has been activated.
  • Allow the tool to cool down. Clean the air vents. Running under no load is still possible.

Disposal

Image alternative Most of the materials from which Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti representative for further information.
Image alternative
  • Do not dispose of power tools, electronic equipment or batteries as household waste!

RoHS (Richtlinie zur Beschränkung der Verwendung gefährlicher Stoffe)

The following link takes you to the table of dangerous substances: qr.hilti.com/r9672135.
You will find a link to the RoHS table, in the form of a QR code, at the end of this document.

Manufacturer’s warranty

  • Please contact your local Hilti representative if you have questions about the warranty conditions.
Image alternative
Image alternative