- Home
- Business Optimization
- News and Events
- Hilti: Partnering up with Red Bull for the Dual Ascent event 2023 at Verzasca Valley Dam, Switzerland
High expectations, high demands
Partner of Red Bull Dual Ascent 2023
Switzerland: Lush forests. Crystal-clear sky. And the massive 220-meter-high concrete wall of the Verzasca Dam looming over the valley.
This is the location of the Red Bull Dual Ascent 2023, the place where 24 climbers in teams of two strive for the impossible.
An exceptional challenge – for Hilti as well: We partnered up with Red Bull for this extreme competition and provided professional tools and anchors to safely install the route.
Check out the climbing route and test the tools yourself at our on-site experience booth. Register here for free tickets and experience the Red Bull Dual Ascent live at the final stage of the competition on November 4th.
climbing up
in a multi-pitch competition
made up of 24 of the world’s best climbers
battling head-to-head
for serial anchor installation
with Hilti SafeSet technology
cured concrete
hardened 2.4 times
The wall that challenges all
For the athletes, one thing is crucial for success: absolute concentration and peace of mind. They need to trust the route installation unconditionally to push their performance to the max.
We took on the challenge to keep the athlete teams worry-free: With high-performance tools, our expertise and anchors that have a proven track record.
Setting-up the route is a though job: 180 meters of vertical mounting, time-pressure, working on the hard concrete while exposed to the weather and installing around 12.000 fastening points are just some of the challenges, the route-setters are confronted with.
Heli Putz
Outdoor Event Organizer
Conquering the wall
The dam’s concrete presents a formidable challenge in its own right. After 60 years of curing, it has hardened 2.4 times its original strength. Interspersed within are blocks of gneiss rock: Their hardness surpasses that of concrete and is comparable to steel. This means that powerful tools and drill bits are needed to prepare the climbing route in such extreme conditions. With our all-new Hilti 22 Volt Nuron cordless battery system, the installation crew can work flexibly, with advanced safety features and reduced need to replace batteries.
When drilling into the hard concrete, TE 6-22 rotary hammer drill with our TE-CX drill bits delivers fast execution speed and high power without compromising on compact, comfortable weight. Active Vibration Reduction and Active Torque Control brings safer application and less fatigue for the installation crew when drilling the high amount of holes. With Hilti’s long battery reach, we also allow for less battery exchanges throughout the application.
Explore Nuron
Overcoming limitations
Anything that saves time and weight is extremely helpful when you are hanging in an awkward position on a 220-meter wall, exposed to the heat. One thing that saves a lot of time is the Hilti SafeSet system: it eliminates time consuming yet critical for the performance steps during anchor installation for a faster, simpler and safer anchor installation such as cleaning the borehole, torquing the expansion anchor, injecting the appropriate volume of chemistry.
This year, the crew used our latest innovation HUS4 MAX Hybrid for anchoring: Drilling the holes, inserting the capsule and driving the screw in with SIW6 – and it’s done.
Explore SafeSet
A strong anchor for the climbers
Another big advantage: The installation crew can save time and tools. The HUS4-H Screw Anchor combined with the HUS4-MAX pre-dosed chemical capsule is a game-changer in fastening technology combining the best of mechanical and chemical properties.
HUS4-H is a mechanical anchor that is very easy and fast to install compared to traditional wedge anchors. No cleaning, no torquing, no hammering, easy to remove – making it ideal for this event specifically, where the fastenings are temporary.
Combined with the HUS4-MAX the Hybrid anchor takes all the speed and easiness of installation: while getting the performance of a chemical injection mortar, you are gaining installation time up to 4 times faster than traditional injection mortar. It is the only chemical anchor solution that doesn’t need cleaning nor curing and that is fully removable after the competition.
Explore HUS 4-MAX
Q&A WITH OUR HILTI EXPERTS
If you can’t watch the thrilling competition on site, join our Instagram live streaming event on November 3rd. – just follow us and switch on notifications.
Learn more about the extraordinary route preparation and the product range during our interviews with Hilti experts.