Fixings timber to block work

Posted by Gary Goddardover 1 year ago
Fixings timber to block work

I need countersunk fixings of 38mm hardwood battens to blockwork in cyclonic areas.

Masonry fixings 2.0kN,timber to masonry

1 Reply
Posted by Mariana Onetoover 1 year ago
Hilti Verified

Hi Gary,

Thank you for your question.

To be able to more precisely suggest an anchor for your application, more information would be required. Therefore, I suggest you reach out to our technical support team >> Technical Advice Services - Hilti Australia

Please find below the important information that are required to support with masonry applications:

  • What type of block are we considering? Hollow, core filled, clay, concrete. What is the resistance of the blocks?
  • What will be the geometry of the fixing? Distance between anchors, diameter?
  • What are the loads of the timber being fixed?
  • Is this a temporary or permanent application?

Other questions might be asked depending on the answers to the above.

Just to suggest an option, our premium fixing for masonry is the HY 270 which has specific ETA approvals for this application in many different types of blocks >> HIT-HY 270 Adhesive anchor - Chemical anchors - Hilti Australia

I hope the above is helpful.

Kind regards,
Ask Hilti team

HY 270,masonry