LIMITED-TIME OFFERGet 20% Off ALL Inserts with code INSERTS20*Shop Now

Solve Labour Issues with the Right Construction Equipment

12-02-2026
Hilti Australia
Reading time: < 5 minutes
Best Practice

Labour shortages slowing your construction projects? Discover how Hilti tools boost productivity, enhance safety, and save time on site. From smarter performance to versatile equipment, learn the 4 key factors that help you do more with fewer workers.

Workforce on Site

Choosing the right construction equipment is crucial for a project’s success — especially today, as the construction industry faces a labour crunch, an aging workforce, and a shortage of skilled workers.

In the past, performance and productivity were the main factors when selecting equipment. But as technology advances and safety becomes increasingly important, there are more considerations to ensure your workforce is fully equipped.

Before we dive into these factors, let’s quickly clarify the difference between tools and equipment…

What's the difference between Tools and Equipment?

Tools v Equipment

We often hear “tools” and “equipment” used interchangeably — but there’s a difference.

In construction:

  • A tool is a single item used to get the job done. For example: “I need to drill into concrete” → you need a cordless combihammer.

  • Equipment is a set or range of tools. For example: “I have the 12V cordless range in my tool park.”

Now, let’s dive in! Here are 4 key factors to consider when choosing construction equipment:

Application-Based Performance

When assessing performance, start with the application — what does the job involve, what materials are you working with, and how long will it take?

For example, if you need to cut curb stones and paving slabs with a material depth of 120mm, the choice narrows to the DSH 600-X petrol saw. Its innovative arbour design allows this blade size to cut the slab in one go. The smaller blade saves money and makes the saw light and compact for its performance class.

If you’re working solo on-site, speed and efficiency are critical. Site rules may also require water when cutting concrete. Hilti’s self-priming pump distributes water at the same speed as the blade, making the DSH 600-X the optimal solution.

On-Site Productivity

Productivity in construction is measured by input (hours worked) vs. output (gross value added).

Consider the bigger picture: how do different tools and features interact with your application? A holistic approach can save time and reduce costs, especially when deadlines are tight.

Ask yourself:

  • What makes this tool more productive than others?

  • Can it reduce time to complete a job?

  • How many workers are needed to operate it?

Safety Features

Health and safety are non-negotiable when selecting tools.

For example, with an angle grinder, features like Active Torque Control (ATC) stop the tool from spinning uncontrollably if the disc jams, reducing safety hazards.
Hilti Smart Power automatically adjusts power output to suit the material, ensuring consistent performance while protecting the motor from overload.

Tool Versatility

A versatile tool can handle multiple tasks, saving time, money, and storage space.

For a construction worker with varied jobs, choosing equipment that covers several applications can streamline your tool park and eliminate redundancy.

Understanding key construction terms can help you choose the right equipment for your job. Here are some important examples:

  • Hand Arm Vibration Syndrome (HAVs): A condition caused by prolonged exposure to vibration, often appearing as vibration white finger or carpal tunnel syndrome, sometimes in as little as 6 months.

  • Exposure Limit Value (ELV): The maximum vibration an employee can be exposed to in a single day.

  • Exposure Action Value (EAV): The daily vibration level above which employers must take action to protect workers.

  • Active Vibration Reduction (AVR): Technology designed to reduce long-term vibration exposure for the user.

  • Active Torque Control (ATC): Advanced sensors and a motor brake that prevent kickback by stopping the tool if a drill bit snags.

  • Dust Removal Systems (DRS): Systems that collect harmful dust using high-performance vacuum cleaners, keeping the worksite safer.

Even with ongoing construction labour shortages, knowing the right tools and technology can boost efficiency, safety, and productivity on site. Now that you understand the essentials, it’s time to put them into action — and Hilti has the equipment and solutions to help you get the job done smarter, faster, and safer.