Incorrect weld strength

Posted by Austin Phamover 1 year ago
Incorrect weld strength

Hi

I just realised that Hilti profis using the strength (fu) of the connected steel to compute weld strength, not the strength of weld material. In the example below, weld material fuw=490MPa, but the weld capacity is checked with fuw=320MPa, which is the fu of steel profile. Can you please explain the reason behind it? Previously I think it used 490MPa which was correct.
Further, it appears that the software only allow to input throat thickness of an integer number, i.e 3,4,5mm... I have weld leg size of 4mm and want to input 2.8mm for throat thickness but not accepted. Can you please clarify?

Thank you.

strength,weld

1 Reply
Posted by Mariana Onetoover 1 year ago
Hilti Verified

Hi Austin,

Thank you for contacting Hilti and for your questions.

Profis Engineering uses the lower strength between the profile and welding material, e.g. in the attached case if the ultimate strength of profile is 500 MPa and ultimate strength of welding material is 490 MPa, then 490 MPa will be used in the calculation (please check attached images).

On your second question, the software allows the input of any throat thickness, e.g. in the attached case of 3.5. It is not necessary to be an incremental value of 3, 4, 5. The reason why you cannot input 2.8mm is because the minimum thickness is to be 3mm as per AS 4100 clause 9.7.3.2 (see attached clause).

I hope the above is helpful, but please contact our Technical Support Services if you have further questions >> Technical Advice Services - Hilti Australia

Kind regards,
Ask Hilti team

Profis Engineering,Weld Strength

1 comment on this reply
Posted by Austin Phamover 1 year ago
Thank you for your answers. Could you please elaborate further the following: (1) On which basis Profis uses the lower of base material strength and weld strength to compute? it seems to me that AS4100 does not specify that. (2) Minimum size of fillet weld as per AS 4100 of 3mm is the leg size, thus I thought the throat thickness of less than 3mm should be allowed. Thanks.