Skip to main content
Cart

At what sizes and type do HUS3-H become seismic C2 performance catagory. I read it is only the HUS3 -HF that is C2 catagory - please can ou clarify.

Posted by William Barrsabout 2 years ago
At what sizes and type do HUS3-H become seismic C2 performance catagory. I read it is only the HUS3 -HF that is C2 catagory - please can ou clarify.

We are looking at seismic design for commercial construction on wall system attachments

Screw Anchor,seismic anchor

1 Reply
Posted by Mohammed Hamdounaabout 2 years ago
Hilti Verified

Hi William,
Thank you for contacting Hilti!

Different varieties of HUS3-H (carbon steel & Hot Dipped Galvanized versions) are approved for both C1 & C2. However, only sizes 8, 10, and 14mm are approved for seismic C2 when installed at the deepest tested embedment depth, hnom 3, as shown under Table C5 on page 26 of the approval document ETA-13/1038, which can be accessed through THIS LINK. Installation parameters for the sizes mentioned above are available under Table B2 on page 14 of ETA-13/1038.

I hope this helps. Please don't hesitate to reach out if you have any further questions.

Best regards,
Ask Hilti Team.