Update of quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
We're always looking to expand and upgrade our product offering to best meet your needs. In fact, all our new tools are developed with input from real construction professionals to ensure each upgrade is bringing something new and valuable to the table.
Cordless tools are a huge part of this, making all sorts of jobsite tasks quicker and easier. That's why, in May, we’re launching a range of new cordless products designed to give Aussie tradies better performance, more versatility, and best in class comfort and ease of use. These are the latest 'must-haves' from our range to keep an eye out for.
An impact driver is one of the key tools found in every tradie's cordless kit. This new tool has been designed with more power, along with increased rotations and more impacts per minute, so screws can be driven in faster. The tool also boasts three gears and electronic speed control, to make switching between driving speeds quick and easy.
Additional features include:
Like the SID 4-A22, this is a tool you'd expect to see on almost every jobsite. The new version features a number of changes over the previous model, including a more compact size and increased power. In addition, there's a new electronic clutch that provides more control and better power delivery. Another big addition is the Active Torque Control (ATC) safety function, which prevents the tool from kicking back and injuring the operator's wrist.
Additional features include:
This is the fourth generation of the Hilti cordless rotary hammer, and brings with it a host of new upgrades that provide increased performance and more versatile functionality. In terms of upgrades, the tool has a new chiselling function and is 30% more powerful. Further, the new brushless motor is more compact and has improved run time. The TE 6-A36 will also now run on the new 36 volt battery platform, providing a choice of batteries to meet the need for lightweight operation or extended run times.
Additional features include:
These are two new products that provide the power of corded grinders combined with cordless mobility needed in high demand applications such as concrete grinding. Utilising the new 36 volt B36 5.2Ah battery, these tools are more powerful and have double the runtime of the 22 volt equivalent The difference between the two tools is the size of the disc, with options of 5 inch or 6 inch.
Features include:
A final addition to the cordless range is two new 36 volt batteries. Choose between 2.6 Ah or 5.2 Ah, depending on the situation and working environment. For example, drilling overhead with the new TE 6-A36 may necessitate the smaller, lighter weight battery, while other applications such as chiselling will need longer run times, which the larger B36/5.2 provides.
A warranty that goes further
Our cordless tools come backed by our unique tool warranty.
Let us manage your tools so you can manager your business
Alternatively, you can choose to lease your cordless tools through our Fleet Management program.
To see account specific prices and content, please choose appropriate account.