Added to cart
Added to cart
Go to shopping cart

Webinar - Risk mitigation in anchor design and installation

In this webinar, we look at ways to mitigate the risk in anchor design and installation. Both factors play a significant role in reducing the risk, and we'll discuss how the right methodology needs to match the appropriate application. We'll look at advances in technology that give designers peace of mind that the specified anchors have been installed correctly, as well as increase installation productivity.In this webinar, we look at ways to mitigate the risk in anchor design and installation. Both factors play a significant role in reducing the risk, and we'll discuss how the right methodology needs to match the appropriate application. We'll look at advances in technology that give designers peace of mind that the specified anchors have been installed correctly, as well as increase installation productivity.

REDUCING THE RISKS

Our February webinar will provide designers, engineers and supervisors with assistance in reducing the risks associated with incorrect installation of anchor systems. Advice will cover deviations to correct installation methods from placement errors, using the wrong products, or using the wrong methods for drilling, cleaning and injecting. The webinar will outline best practices in line with the technical standard SA TS 101 of the National Construction Code.

KEY RISKS

There are a number of risks to be aware of in this process, from initial design all the way through to installation. The risks include but are not limited to: 

  • Drilling into existing services, reinforcement materials or voids in the concrete
  • Using non-approved products.
  • Specifying a product that isn't compatible with the drilling method.
  • Installers changing a product without notification.
  • Holes not being cleaned according to approval documents.
  • Chemical resins not in line with the correct methodology.
  • Mechanical anchors not using the correct torque.
  • Anchors are too long for the thickness of the concrete.
  • Anchors being reused without approval.
  • Generating excess dust.

BENEFITS FOR TAKING PART

This webinar presents a great opportunity for design and quality verification engineers, product specifiers, and project managers to improve existing knowledge around mitigating risk in anchor design. You can never be too careful, and this is an area where a wider knowledge is hugely beneficial to ensuring timely, efficient project completion.

After attending this webinar, you will receive an attendance certificate via email. Hilti webinars are eligible for CPD points, helping you on your way to further career opportunities.

WHEN IS THE WEBINAR AND WHEN DO I SIGN UP ?

To register, all you need to do is click on the link for your preferred session below, fill in your details, and then join the webinar on the day. As with all Hilti webinars, we'll have a team of engineers available via live chat to answer questions during the presentation.

OUR PRESENTER

Mike Coburn is a Senior Field Engineer at Hilti. He has worked across a broad mix of civil projects, commercial and residential buildings.

Mike holds a Civil Engineering degree from the University of Sydney and is a member of Engineers Australia.

CONTACT US
CONTACT US