Update of quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
The local authority in Pune commissioned a new bridge over the river to smooth out traffic flow in the city.
During the late stages of the project, the position of light poles and the design of the railings were changed.
The project manager had to find a solution which could meet tight deadlines but also could cope with a low embedment depth for the anchors.
Our local Hilti engineers suggested using our Hilti HVA anchors for fixing the light poles and our Hilti HST anchors to fix the handrails.
Both were approved by the design engineers and incorporated into the bridge build.
Our local Hilti team gave technical support during the design phase. This helped to ensure that the stringent shock load requirements were met. We also gave support onsite during the build.
QUICK LINKS
RELATED SOFTWARE
Ask an engineer
To see account specific prices and content, please choose appropriate account.