Added to cart
Added to cart
Go to shopping cart

Crown Apartments, Mackay

Facade panels and windows secured with Hilti HUS screw anchors

The Challenge

This nine-storey apartment building in Mackay required a new waterproofing facade system of approximately 2,000 square metres - including new windows. The retrofitted facade consisted of James Hardie ExoTec facade panels, which were fixed to steel battens over a waterproof membrane.

The Solution

The structural engineering consultants from Flanagan Consulting Group and Sydney-based main contractor Polyseal Waterproofing Pty Ltd chose Hilti HUS-HF 10x80 and HUS-HF 10x100 hot-dipped galvanised screw anchors for fixing the steel battens to the existing Dincel wall. For all windows on the building, Hilti HUS-HR stainless steel screw anchors were selected.

Our HUS screw anchors were chosen for this project because of their excellent load rating on the existing wall system (containing regular 30 millimetre voids) as well as their corrosion resistance, essential for this seaside location. The fast and simple installation process of our screw anchors results in huge time and cost savings when fixing in excess of 50,000 anchor points, which was another important deciding factor in choosing Hilti products for this construction.

 

Top Hat battens secured using hot-dipped galvanised Hilti HUS3 screw anchors

Top Hat battens secured using hot-dipped galvanised Hilti HUS3 screw anchors

Steel window lintels secured using stainless steel Hilti HUS3 screw anchors

Steel window lintels secured using stainless steel Hilti HUS3 screw anchors

Proof Testing the HUS3 screw anchors on Crown Apartments, Mackay

Proof Testing the HUS3 screw anchors on Crown Apartments, Mackay

Waterproof façade installed with Hilti HUS3 screw anchors

A job well done. Quick and easy façade installation with HUS3 screw anchors

Ask an engineer

Log in to proceed
Need help? Contact us
Register Here
CONTACT US
CONTACT US