How innovative technologies can save time and increase efficiency

Making penetrations for mechanical and electrical services

For any mechanical or electrical contractor - we're talking everybody from plumbers to air conditioning installers to electricians here - there is often a need for penetrations to be made in a surface or masonry wall. This could be for any number of reasons, ranging from running a cable or pipe through to installing a particular part, for example an electrical socket. Regardless of the reason for a penetration’s requirement, there can be a few issues that crop up when attempting to drill one, and this is particularly the case with any holes that need to be larger than about 20 millimetres in diameter.

Making penetrations can be some of the most delicate work that you will do on-site, and this is a problem because spending time drilling holes isn't what you are there to do. By speeding up the process and making it simpler, it is possible to work faster, creating more time to focus on the trickier technical parts of the job.

In this article, we'll take a look at why making holes has proved to be a problem in the past, and how new products from Hilti will ensure this isn't the case in the future.    

Please enter alternative text here (optional)

The trouble with penetrations

Our wide variety of drill bits give tradies all the options they need in terms of hole size.

There are a few different options you have when trying to make larger holes. You can use a physically bigger drill bit, or a more specialist piece of equipment such as a diamond corer, but all of these methods are still relatively complicated. Hilti Trade Manager Martin Stirling describes the whole process as a "headache," and something that needs to be refined for contractors to work more efficiently.

"It's fiddly, and anything that's got the word 'fiddly' associated with it is time-consuming, and therefore very expensive when you look at labour costs," he said.

Here at Hilti, our focus is on making a difference to your work, and one of the ways that we can do that is by making processes like this one easier and more productive. With this in mind, we've developed a range of products and solutions that allow you to make penetrations quickly through any wall type - be that masonry, plasterboard or concrete.

Some of these are our wide variety of drill bits, which give you all the options you need in terms of hole size, but we've also put a lot of thought into the practicalities of actually making a penetration. For example, dust extraction accessories can be easily mounted to many of our tools, meaning that a big hole can be drilled in a virtually dust-free environment. Not only does this make the drilling easier and safer, but it also limits cleanup time afterwards.

One of the most exciting developments, however, is the upcoming launch of our new percussion core bit, the TE-C-DS.

The Hilti TE-C-DS percussion core bit

Please enter alternative text here (optional)

The TE-C-DS is a hybrid between a core bit and a hammer drill bit, which allows for large holes to be drilled very quickly with a minimal amount of dust. This bit boasts all of the features you need to make penetrations as efficiently as possible, and we at Hilti are very excited about the impact this product will have on Australian sites.

"It would normally take half an hour for people to make the hole and then put a cable through or put a power socket in," said Martin, "but you can get that down to virtually minutes."

Essentially, what the TE-C-DS offers to contractors are immense time savings. This benefits you, as you can get more work done, along with your clients who don't have to pay for time spent drilling holes.

Martin describes this drill bit as "revolutionary," and it's easy to see why. There are other products out there, namely diamond hole saws and corers, that can perform a similar function, but these are either messy (when using water), or very time consuming.

“If contractors are forced to make a compromise between speed and long cleanup times, then we don't believe that the solution is satisfactory, and the TE-C-DS provides the best of both worlds,” he summarised.

One of the biggest issues for tradies when it comes to tools is cost, and it isn't practical or affordable to be always upgrading to a different system whenever a new drill bit comes out. For that reason, the TE-C-DS is compatible with the SDS Plus connection end, which Hilti helped to develop in the 1970s and is still immensely common today.

This means that the TE-C-DS works with any Hilti tools that use this standard, so smaller tools can be used rather than having to haul around a large diamond core rig. These tools are also cordless, which makes it even easier for you to quickly carry out the necessary penetrations and then get on with the rest of your work.

The TE-C-DS is a big leap forward for the mechanical and electrical trades, and you can contact Hilti today to find out more about it.

Long lasting batteries make cordless tools an integral part of every jobsite

Long lasting batteries make cordless tools an integral part of every jobsite

How cordless tools can save time for Australian tradies

See how cordless can save you time

Please enter a subline

Please enter link

Everything you need to know about designing post-installed rebar

Post-installed rebar can be just as safe as traditional cast-in reinforcement but the design phase is a critical part of the process to getting it right.

Learn about post-installed rebar design